Ultimate Initio 4WD Robot Platform
for Raspberry Pi with RoboHAT
The Ultimate Initio is a 4WD robot platform that is ideal for use with Raspberry Pi single board computers.
The platform is a doddle to assemble and easy to use and comes with the RoboHAT robotics board and
an assembled 2DOF pan-tilt servo assembly, as well as a number of other sensors that make this platform
L_[YLTLS` ÅL_PISL HUK WLYMLJ[ MVY H ^PKL YHUNL VM WYVQLJ[Z
The main chassis comes pre-built, with the wheels, motors, gearboxes, battery box and wheel sensors
all in place. The powerful 170-size motor is coupled to a high-quality gearbox and there are built-in speed
encoders on each side. Each wheel can be individually decoupled from the gearbox so you can run the
robot in 1WD, 2WD or 3WD modes if you want.
Kit contents:
• Main Initio chassis (with wheels, motors, gearboxes, battery box, wheel sensors, screws and all mountings)
• RoboHAT Robotics Controller Board 75-0284
• Pan-Tilt 2DOF assembly with servos (ready assembled)
• 2x IR Obstacle sensors
• 2x IR Line sensors
• 1x Ultrasonic sensor
• All connecting cables as required for above items
• Build instructions and example code can be found on the 4tronix website.
Note: Raspberry Pi and batteries not included.
Pi2Go Raspberry Pi Robot
Inc. Motors, Sensors and
Driver Board
If you’re hungry for some robot action then the Pi2Go
is the beast for you. The Pi2Go is the complete
robot for use with your Raspberry Pi and supports all
TVKLSZ L_JLW[ [OL ]LY` ÄYZ[ YLSLHZL ^OPJO OHZ UV
mounting holes): Model A, Model B, Model A+, Model
B+, Pi 2 Model B and Pi 3 Model B. Assembly is quick
and simple, with no separate chassis - everything
is connected to the main circuit board. There is no
ZVSKLYPUN VY NS\PUN YLX\PYLK [OL HZZLTIS` Q\Z[ ZJYL^Z
together.
For software, a python library module is available that
has some example programs that will demonstrate:
• Move motors forwards, backwards, spin left/right
or do sweeping turns
9LHK [OL ]HS\LZ MYVT HSS [OL 09 ZLUZVYZ 6U VY 6ќ
• Read the distance using the ultrasonic sensor
• Read the value of the switch
• Set the RGB LEDs to any colours you want
• Set the position of each servo
Visit the Pi2Go website for assembly details, software
downloads and news updates.
Note: Raspberry Pi and batteries not included.
Order code
75-0283
£55.00
Order code
75-0287
£2.95
Order code
75-0286
£5.00
Order code
75-0284
£19.95
Order code
75-0285
£13.30
Order code
75-0282
£95.00
,K\JH[PVUHS ;YHɉJ 3PNO[
for Raspberry Pi
The Pi-Stop
PZ HU LK\JH[PVUHS [YHѝJ SPNO[ WYVQLJ[
for Raspberry Pi. The low cost hardware module
is designed to allow you to use your Raspberry Pi
[V [HRL [OL ÄYZ[ Z[LWZ PU[V PU[LYMHJPUN ^P[O [OL YLHS
^VYSK @V\»SS IL VU [OL ÄYZ[ Y\UN VM [OL 0U[LYUL[ VM
Things ladder as soon
as the lights change to
green. The brilliant thing
about the Pi-Stop is the
familiarity of the elements,
everyone knows what
they are and how they
can be used.
Note: Raspberry Pi
not included.
RoboHAT Robotics Controller
Board for Raspberry Pi
The RoboHAT is the complete robotics controller for
your Raspberry Pi based mobile robot. The board
supports all models of Raspberry Pi that have the
40-pin connector (Model A+/B+, as well as Pi 2
and 3 Model B).
•
Supplied fully assembled
•
Perfect with Pi
•
Python library module for super-easy use
PZM Motor Controller Shim
for Raspberry Pi Zero
The PZM Pi Zero Motor Shim is a brilliant way of
adding motor control to (almost) any Raspberry Pi
WYVQLJ[ (S[OV\NO ZWLJPÄJHSS` KLZPNULK MVY \ZL ^P[O
the Raspberry Pi Zero, the board can be used with
any other Pi.
•
PZM Shim supplied ready assembled
•
Mount with supplied headers
•
Or solder directly to bottom of Pi header
•
Reverse polarity protection
PiStep2 Dual/Quad Stepper
Motor Controllers for
Raspberry Pi
These stepper motor control boards are designed
for use with all versions of the Raspberry Pi with the
40-pin GPIO connector. The boards are available
in dual (2 steppers) or quad (4 steppers) versions.
•
Fully assembled - no soldering required
•
Raspberry Pi Zero form factor
•
Each pin has an associated LED to see
stepper signals
Note: Stepper motors and Raspberry Pi not included.
Dual
Order code
75-0288
£8.00
Quad
Order code
75-0289
£10.50
Picon Zero
0U[LSSPNLU[ 9VIV[PJ
Controller for
Raspberry Pi Zero
The Picon Zero is an intelligent robotics controller
designed for your Raspberry Pi Zero. It supports
all models of Raspberry Pi with a 40-pin connector
(Zero, Model A+/B+ and Pi 2 or 3 Model B).
The built-in processor handles all the direct
communication with your input and output devices,
leaving you to worry about the overall control with
your Raspberry Pi program.
For full details and to see our full range of 4Tronix products visit
www.rapidonline.com/4tronix6
Raspberry Pi
6
Education
Tel: 01206 751166 Fax: 01206 751188
Raspberry Pi