11
www.rapidonline.com/tools-equipmentE V E N MO R E T O O L S AVA I L A B L E
Ultrasonic cleaning is a unique phenomenon.
Millions of tiny bubbles are created when ultrasonic sound is passed
through a liquid. These tiny bubbles, combined with sound pressure,
give brilliant cleaning results.
For best results, the
manufacturer recommends
the use of JPL Sea Clean
cleaning solution. They
cannot guarantee the
effectiveness of other
cleaning solutions. Please
check before using that
items to be cleaned are
suitable for ultrasonic
cleaning, e.g. specialised
lens coatings on spectacles.
Ultra 2000 Compact
420ml
The JPL Ultra 2000 compact ultrasonic
cleaner has a 420ml tank and can
clean a host of items including jewellery,
waterproof watches, spectacles, razor
heads, dental equipment, car and
machine parts, plus much more.
Ultra 7000S 750ml
This 750ml ultrasonic cleaner from JPL
is the perfect way to return your CD/
DVD’s, jewellery and watches back to
new. The number of uses are endless,
from cleaning spectacles/sunglasses to
grubby coins, while model makers will
find it indispensable!
Ultra 7000 with Digital
Timer 750ml
Its control panel has a simple-to-use
digital timer that lets you select your
required cleaning time from one of five
preset times between 90 seconds and
8 minutes.
Ultra 8051 2.5L
This 2.5L ultrasonic cleaner from JPL
is the perfect way to return your CD/
DVD’s, jewellery and watches back to
new. The number of uses are endless,
from cleaning spectacles/sunglasses to
grubby coins, while model makers will
find it indispensable!
Ultra 8050D-H
Professional 2.5 Litre
The Ultra 8050-DH also has a built in
heater, which when programmed, will
heat the water to a useful 65°C, further
enhancing your cleaning capability. The
cleaner is supplied complete with a
basket to hold your smaller items.
Ultra 9020 6L
The control panel of the Ultra 9020
cleaner has a simple to use digital timer.
Set your required cleaning time between
1-30 minutes, and let the cleaner do the
hard work for you. Despite the compact
size, the Ultra 9020 has a large 6L tank.
The basket will carry many small items,
saving time and keeping them secure.
Ultra 8060D-H 3 Litre
The Ultra 8060 has a range of options
and features to give you the best results
from your cleaning: a built-in heater,
quiet operation technology, digital timer,
powerful 150W Ultrasonics, de-gas
function (de-gassing helps remove
the oxygen from the fluid, making
smaller bubbles which in turn means
more powerful cleaning) and a built-in
drain tap.
Sonic 3MX 160W
High Power 3L
The control panel of the Ultra 3MX
cleaner has a simple to use LCD display.
Set your required cleaning time between
1-60 minutes, and let the cleaner do the
hard work for you. Despite the compact
size, the Ultra 3MX has a large 3L tank.
The basket will carry many small items,
saving time and keeping them secure.
Order code
87-3270
£24.18
Order code
87-3282
£29.99
Order codes
500ml
87-3278
5 litre
87-3280
£4.80
£24.22
Order code
87-3272
£27.95
Order code
87-3284
£95.74
Order code
87-3274
£95.93
Order code
87-3286
£239.96
Order code
87-3276
£121.19
Order code
87-3288
£257.99
Sea Clean 2 Double Strength Concentrated Cleaning Fluid
A high-powered and versatile cleaning solution that gives amazing results when used in conjunction
with an ultrasonic cleaner. It is made from a unique blend of natural products, mixing carefully balanced
quantities of seaweed, coconut oils and fruit extracts to create a powerful cleaning solution.
SeaClean2 will brilliantly clean tarnished items and assist in
the removal of carbon, rust and dirt from most jewellery, tools,
mechanisms, sporting goods and can even un-block injket
cartridges.
•
Long shelf life - 12 months from opening bottle
•
Available in 500ml and 5 litre bottles
For full details visit
www.rapidonline.com/james-products