Background Image
Previous Page  23 / 36 Next Page
Information
Show Menu
Previous Page 23 / 36 Next Page
Page Background

21

21

www.rapidonline.com education@rapidonline.com

Physics

One Metre

Wheatstone

Bridges

Wheatstone bridges allow accurate

comparison of two resistances

by sliding a ‘jockey’ contact along

a metre length of ‘resistance wire’.

When a balance is achieved,

indicated by a zero reading

on a galvanometer (not included),

the position of the jockey on

the wire, gives an indication

of the ratio of the two fixed

resistances. If the value

of one of the fixed resistances

is known, the value of the

other can be inferred.

These substantial bridges

have broad, heavily plated

brass strips mounted on

a polished hardwood base.

Terminals with 4mm sockets are provided.

24 SWG constantan wire is stretched along the

top of a metre scale graduated in mm and cm.

•

Supplied with jockey

•

Dimensions 1.13m x 80mm x 5mm approx.

•

Available in 2-gap and 4-gap models

•

Eisco PH1156 series

Type

Order code

1+

Four gap bridge

52-3627

£29.95

Two gap bridge

52-3628

£24.95

565651

Parallel Plate Capacitor

Demonstration

This demonstration capacitor consists of two 120mm circular metal discs mounted

on insulated supports that slide on a track to adjust the distance between them.

The distance can be easily measured by reading their respective positions on the fixed scale.

The apparatus allows students to observe the principle of capacitance, its relationship with charge

and voltage, its dependence on the surface area of conductors and the dielectric medium between two plates.

The apparatus is supplied with three different dielectric materials: glass, cardboard, and Lucite.

•

Sturdy extruded aluminium section

•

Eisco type PH0879

Electromagnet

The Eisco PH0800A electromagnet consists of

a U-shaped iron core of circular section, with

armature and carrying hook. It is wound with

insulated copper wire and provided with colour-

coded 4mm connectors.

•

For use on 4 to 6V DC

•

Eisco type PH0800A

Crookes Radiometer

This radiometer consists of a partly evacuated

glass bulb approximately 70mm in diameter,

containing a fine pivot which supports four light

weight metal arms. One side of each vane is

blackened, the reverse side is bright.

On exposure to sunlight, or a sufficiently bright

incandescent light source, the vanes turn. The

absorption of radiant energy by the blackened side

of the vanes sets up a temperature differential with

respect to the bright sides, causing net force to

be exerted by the air molecules on the blackened

side which makes the vanes rotate with their bright

faces leading.

•

Approx. 70mm diameter

•

Mounted on round plastic moulded base

•

Eisco type PH0418A

Demonstration

Meter

Used to demonstrate the working

principle of AC or DC ammeters

or voltmeters, the

meter is housed in a

300 x 150 x 30mm

ABS plastic case

with glass front and

rear panels.

•

Moving coil type

•

Accuracy of ±

2.5%

•

Basic sensitivity

5mA

•

100mV f.s.d. (full

scale deflection)

•

Eisco type

PH1116

Demonstration

Dynamo with

Hand Pulley

This working model dynamo is mounted on a 200 x

125mm base plate, which also supports a 125mm

diameter hand-driven pulley. The pulley is coupled,

via a rubber belt, to a smaller pulley on the dynamo

shaft, providing a step-up ratio of rotational speed.

Electrical output is via a pair of 4mm sockets and

a light emitting diode is provided as a simple output

indicator. The model can also be used as a motor

when connected to a 6 to 8V DC supply (not included).

•

Electrical output via 4mm terminals

•

LED output indicator

•

Can be used as a demonstration motor

(requires 6 to 8V DC power supply)

•

Includes instruction manual

•

Eisco type PH1246

Order code

52-3635

£34.95

Order code

52-3338

£42.95

Order code

52-3443

£24.95

Order code

52-3310

£5.99

Order code

52-3332

£5.95

…where price meets quality