Background Image
Previous Page  25 / 36 Next Page
Information
Show Menu
Previous Page 25 / 36 Next Page
Page Background

23

23

www.rapidonline.com education@rapidonline.com

Physics

Snell’s Law

Spouting

Cylinder

An apparatus for demonstrating

the principle of Snell’s Law,

which states that pressure

increases with depth.

Liquid will exit from the 3 spouts

and travel further horizontally

depending on the depth of liquid

above them.

•

60mm diameter acrylic pipe

•

400mm total height

•

3 spouts at predetermined

heights

•

Eisco type PH0196

Equality

of Liquids

Apparatus/

Pascal’s Law

Syringe

An apparatus consisting of a glass

flask with holes in the bulbous part

and a glass piston that slides in the

straight part.

When filled with liquid, the piston is

pushed into the apparatus, causing

liquid to exit each hole with equal

pressure regardless of the hole’s

position or direction.

•

Also known as Pascal’s Law

syringe

•

Eisco type PH0194

75mm Brass

Magdeburg

Hemisphere Set

A practical vacuum and

atmospheric pressure

demonstration set consisting

of two 75mm diameter brass

hemispheres.

Each hemisphere has a handle firmly attached

to it. One of the hemispheres has a stopcock

for attaching to vacuum tubing. When the

hemispheres are pushed together and evacuated

using a vacuum pump they are hard to pull apart.

Get 2 students to pull, then open the stopcock to

let air in and the hemispheres will separate easily

to the surprise of the students.

•

Made of brass

•

Fitted with stopcock

•

Diameter 75mm

•

Eisco type PH0172

Vacuum Pump Plate

This pump plate has been manufactured from aluminium and has

a tube for connection to a vacuum pump and a stopcock for air

regulation.

The plate is mounted on a heavy, painted tripod base for good

stability and is supplied with a rubber seal which facilitates sealing in

experiments involving bell jars.

•

Diameter 250mm

•

Tripod-style base for stability

•

Suitable for many physics experiments involving a vacuum

•

Eisco type PH0156C

Hand-Powered

Vacuum Pump

This economical vacuum pump features a

gauge graduated in both cm³ and inches³. Each

depression of the handle displaces 15ml of air.

•

Economical vacuum pump

•

Gauge in cm³ and inches³

•

Maximum vacuum 50mm of Hg

•

Can also produce positive pressures up to 2atm

•

Pump rate 15ml per stroke

•

Clear tubing is 600mm long with 6mm inner

diameter

•

Eisco type PH0167

Jolly Bulb with Gauge

This Jolly bulb apparatus consists of a 60mm diameter

bulb directly connected to a bourdon pressure gauge.

The apparatus is used for investigation of gas at a

constant volume. By inserting the glass bulb into either

warm or cold water, the expansion or contraction of

the air contained in the bulb can be seen as a pressure

change on the gauge.

•

60mm diameter glass bulb

•

Gauge calibrated in both kg/cm² and in psi

•

Eisco type PH0138C

Order code

52-3360

£34.95

Order code

52-3329

£9.95

Order code

52-3330

£4.79

Order code

52-3361

£27.95

Order code

52-3331

£24.95

Order code

52-3700

£29.95

Type

Order code

1+

Solar cell & motor

52-3353

£24.95

Solar cell only

52-3354

£13.49

Solar motor & fan

52-3355

£9.35

565540

Solar Cell and Motor

Demo Set

A range of solar units, ideal for

demonstrating the conversion

of solar energy into mechanical

energy.

•

Range includes solar cells,

solar motors, LED and buzzer

6 days per week

phone orders

Monday to Friday 8am to 7pm

Saturday 9am to 5pm