Background Image
Previous Page  33 / 36 Next Page
Information
Show Menu
Previous Page 33 / 36 Next Page
Page Background

31

31

www.rapidonline.com education@rapidonline.com

Physics

Resonance

Apparatus

with Telescopic

Brass Tube

This resonance apparatus is comprised

of two brass tubes that can telescope

into each other, allowing the column of air

within the tube to be varied between 300 and 530mm.

•

Outer tube fits into base

•

Eisco type PH0718B

Resonance Tuning Forks with Hammer

This apparatus can be used for demonstrating the production of beat frequencies.

It is comprised of two nickel-plated tuning forks mounted on individual sound

boxes. The two forks both produce an ‘A’ note (440Hz) when struck with the

mallet. One fork is provided with an adjustable mass, by means of which

the frequency of that fork may be shifted from the nominal 440Hz.

When both forks are sounded at the same time, a clearly audible

‘beat’ is produced, its rate depending upon the difference

in frequency between the two forks.

•

Used to hear dissonance

•

One fork adjustable

•

Supplied complete with 2x tuning forks, 1x adjustable

mass, 2x bases and mallet

•

Eisco type PH0742A

Tuning Forks Set

An eight-piece set of nickel-plated

tuning forks with plain shanks. The

forks are marked with their individual

frequencies: C (256Hz), D (288Hz),

E (320Hz), F (341Hz), G (384Hz), A

(426Hz), B (480Hz) and C (512Hz).

•

8-piece set

•

Supplied in wooden storage case

•

Eisco type PH0738B

Order code

52-3342

£21.49

Order code

52-3436

£25.95

Order code

52-3698

£14.95

Set of 6

Tuning Forks

A range of superior quality aluminium

tuning forks with plain shanks and

round stems.

•

Ideal for school, college and

laboratory use

•

Eisco PH0737 series

Note Frequency

Order code

C

256Hz

52-3453

D

288Hz

52-3454

F

341Hz

52-3455

G

384Hz

52-3456

A

426Hz

52-3457

B

480Hz

52-3458

C

512Hz

52-3459

565598

Tuning

forks

£3.89

Each

Cubes for Density

Investigation Set

A set of six 20mm cubes fitted with a hook

for easy handling. Each cube by definition has

identical volume but widely differing weight.

Materials include: brass, lead, zinc, copper,

aluminium and iron.

•

Supplied as a

set of 6

•

Eisco type PH0108P

Specimen Density Set

A set of 25mm cubes of various materials for

density investigation. Each cube by definition has

identical volume but widely differing weight.

The set includes: brass, iron, copper, aluminium,

hardwood, softwood, nylon, PVC and acrylic.

•

25mm cubes

•

Wooden storage box

•

Supplied as a

set of 9

•

Eisco type PH0109A

Leslie’s Cubes

These Leslie’s cubes have sides with different

surface finishes. They are ideal for use in

experiments to show how objects emit and

absorb heat.

In use, the apparatus is filled with water which is

maintained at boiling point by a low Bunsen burner

flame. Infra-red sensors, etc., can be used to

compare the relative radiant heat output from each

of the four faces.

•

Top hole for filling and emptying

•

Bung for thermometer

•

Eisco PH0411 series

Size

Material

Order code

1+

100mm

Copper

52-3650

£13.95

130mm

Tin

52-3649

£7.99

565658

Order code

52-3702

£24.95

Set of 9

Order code

52-3446

£12.99